Technical FAQs

Ask a Question

Unity Simulator Communications capability

Title
Unity Simulator Communications capability
 
Issue
Unity Simulator Communications capability
 
Product Line
Unity Pro
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The Unity Simulator does not have the capability to initiate communication out of a Network Option module installed in the program.
Also, The Unity simulator does not have the capability to initiate communication with devices configured in the DTM Browser.
The Unity Simulator only simulates the program logic.
 
Was this helpful?
What can we do to improve the information ?