Technical FAQs

Ask a Question

M580 DTM Browser Device Active Configuration

Title
M580  DTM Browser Device Active Configuration
 
Issue
M580  DTM Browser Device Active Configuration
 
Product Line
M580
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
When setting up DIO devices on an M580 through the DTM Browser, you can turn off the "Active Configuration" in the Unity DTM and Unity will remove that device from the Unity Pro project configuration. 
But the DIO device details will still be in the Unity DTM Browser listing but it will not be communicated with.

 
Was this helpful?
What can we do to improve the information ?