Technical FAQs

Ask a Question

M580 BMENOC03x1 and RSTP


Title
M580 BMENOC03x1 and RSTP
 
Issue
M580 BMENOC03x1 and RSTP support
 
Product Line
M580 BMENOC0301 BMENOC0311
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The BMENOC03x1 Service Port (ETH1) does not run the Spanning Tree (STP/RSTP) protocol.
However , BMENOC03x1 Ethernet port 2 (ETH2) and port 3 (ETH3) do use the Spanning Tree (STP/RSTP) protocol.
 
Was this helpful?
What can we do to improve the information ?