Technical FAQs

Ask a Question

Does the BMXNOR0200 support an Email Client service?


Title
BMXNOR0200 Email Client service
 
Issue
BMXNOR0200 Email Client service
 
Product Line
BMXNOR0200H
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 Yes the BMXNOR0200 has a Email / SMS service and it is configured using Web Designer software.
NOTE: The SMS feature is supported only when a GSM or GPRS modem is configured. The SMS is sent only when the modem connection is not open.
 Please reference the user manual's Chapter 9 - How to Work with Email/SMS Service.

 
Was this helpful?
What can we do to improve the information ?