Technical FAQs

Ask a Question

Does Unity Pro run on Windows Server 2016?

Unity Pro v13.1 (August, 2018)  is validated to run on Windows 7 32/64 , Windows 10 and Windows Server 2016.
 
Was this helpful?
What can we do to improve the information ?