Browse FAQs

What is the meaning of the suffix "X" on ATV61HD22N4X?

Published date: 28 July 2019

Issue : 
What does the suffix "X" mean on part number ATV61HD22N4X?

Product Line :
Altivar 61 Drive

Environment :
ATV61HD22N4X model only

Cause :
Availability of unit

Resolution : 
The meaning of "X" for the ATV61HD22N4X is to indicate that the unit is in the exchange pool stock of Greensboro Repair Facility. This is a no longer sold unit. We cease production of this in 2016. Only customers with existing units that are still under warranty can make an exchange for a refurbished one from the repair depot. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.