Technical FAQs

Ask a Question

Regarding that the M580 SIL3 Safety processors have been officially released, could you please advise if there are any dates announced for the phase out of the Quantum Safety controller.

The Quantum Safety range is still in Active phase. Idea is to keep it alive until the Redundant M580 Safety will be available.
The Redundant M580 Safety launch is expected Q4/18. So, I think to announce the Quantum Safety End Of Commercialization (EOC) end 2018 with a possibility to postponed it to end 2019.
So, if the EOC announcement is Dec.2018, then the effective EOC will be Dec.2020 and End Of Service (EOS) 2028.
Was this helpful?
What can we do to improve the information ?