Technical FAQs

Ask a Question

Can I acknowledge individual alarms with RealStream remotely using a Modbus Host?

The state of select alarms can be monitored using a Modbus Host. Individual alarms cannot be acknowledged using a Modbus Host.  There is an option to acknowledge all active alarms from a Modbus Host. See the Modbus Register map provided in the configuration manual for more details.
Was this helpful?
What can we do to improve the information ?