Technical FAQs

Ask a Question

How do I check the communication settings of my RealStream Lift Station controller? DNP3 Address, IP Address, Modbus Settings

All of the station communication settings can be configured and viewed from the local display. These can be found by logging in:
-> Main Menu -> 1.6 System Settings -> 1.6.2 Modbus Slave Address -> 1.6.3 RTU IP Address -> 1.6.5 Port 3 Config -> 1.6.6 DNP3 Address -> 1.6.7 Modbus/TCP Server
Was this helpful?
What can we do to improve the information ?