Technical FAQs

Ask a Question

Is it possible to customize switchboards according to the requirement?

Yes, As per the customer requirement it is possible to customize the switchboards (in the Switchboard design tab). Depends on the customer input usually rapsody suggests the switchboard design & customization of the switchboard can be done in Front view of Switchboard design tab.
Was this helpful?
What can we do to improve the information ?