Technical FAQs

Ask a Question

What are the Environmental characteristics of DM6000H meters ?

Environmental characteristics:

Operating temperature:  -10º to +60º C (+14º ... +140º F)
Storage temperature:     -20º to +70º C (-4º ... +158º F)
Humidity rating:               5 to 95 % RH non-condensing
Pollution degree:             2
Attitude:                           ≤ 2000 meters (6561 ft), Category III
Product life:                      > 7 years
Insulation category:          Double insulation for user accessible parts
Location / mounting:         Not suitable for wet locations
 
Was this helpful?
What can we do to improve the information ?