Technical FAQs

Ask a Question

What are the AC control power characteristics of DM6000H meter ?

AC control power

Operating range:  48 to 277 V L-N AC ± 10%
Burden:                 ≤ 4V A at 240 V L-N, 50 Hz
Frequency:            50 / 60 Hz nominal (45 to 65 Hz operating range)
Ride-through time: 200 ms at 240 V L-N, 50Hz (at Ambient condition)
Was this helpful?
What can we do to improve the information ?