Browse FAQs

How to measure block demand in PowerLogic ION meters

Published date: 18 September 2019

Issue
There is no block demand module in ION meter template.

Product Line
ION meters

Environment
Demand Framework (meter template)

Cause
A need to have the meter calculate block demand as opposed to sliding window demand

Resolution
Block demand calculations are completed at the end of each demand interval, and the result is used as the new present value for the peak demand evaluation.
As such, block demand can be measured using the Sliding Window Demand module by ensuring the number of subintervals is set to 1.

          

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.