Browse FAQs

Does the ATV340 drive support Device Level Ring (DLR) technology for Ethernet IP?

Published date: 12 April 2019

 Issue:
Does the ATV340 drive support Device Level Ring (DLR) technology for Ethernet IP?

Product Line:
Altivar 340, ATV340.

Environment:
All serial number, all model number.

Cause:
Customer was working with a supplier to UPS and they have to use Rockwell PLCs, so the question came up.

Resolution:
DLR is not validated for ATV340, our solutions are RSTP based.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.