Browse FAQs

Preventa XCS - How to order the XCSZR790L01M12 part number ?

Published date: 05 June 2019

Find attached the picture of both part XCSZR1 magnet and XCSZR790L01M12 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMR790L01M12. This is the commercial reference to order to get the XCSZR790L01M12 switch with the magnet XCSZR1, sold into the same packaging plastic bag.

Was this helpful?

What can we do to improve the information ?