Browse FAQs

Preventa XCS - How to order the XCSZC790L01M8 part number ?

Published date: 05 June 2019

Find attached the picture of both part XCSZC1 magnet and XCSZC790L01M8 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMC790L01M8. This is the commercial reference to order to get the XCSZC790L01M8 switch with the magnet XCSZC1, sold into the same packaging plastic bag.

Was this helpful?

What can we do to improve the information ?