Browse FAQs

Osisense XC - How to identify the black XCKS limit switch reference to order?

Published date: 06 June 2019

In the XCK limit switches series, the reference of the complete limit switch in standard is not indicated on the product. For the old XCKS series in black color, the body and head are marked on the sub-assemblies with the manufacturing date. See XCKS picture attached: it consists of the ZCKS1H29 body and the ZCKD31 plastic roller lever, so the complete limit switch has the reference to order XCKS131H29. Anyway you can also order the sub-assemblies separately to get the switch.

  

Was this helpful?

What can we do to improve the information ?