Technical FAQs

Ask a Question

Connexium Manged Switch Event Logging capability

Title
Connexium Manged Switch Event Logging
 
Issue
Connexium Manged Switch Event Logging capability and a failed login attempt
 
Product Line
Connexium Managed switches.
 
Environment
Connexium
 
Cause
N/A
 
Resolution
 The Connexium event log records switch process events that occur with the switch's fuctionality
The Connexium event log does not have the capability to log an event that records a successful login nor an attempted login to the switch with an invalid password.
Also, there is no security log builtin to the Connexium Managed switch
 
Was this helpful?
What can we do to improve the information ?