Browse FAQs

SEND_REQ Request code 16#9F

Published date: 30 September 2019


Title
SEND_REQ Request Code 16#9F
 
Issue
SEND_REQ Request Code 16#9F used for Modbus
 
Product Line
M580
 
Environment
Unity Pro

Resolution
The SEND_REQ request code 16#9F is used indicate that the request is a Modbus type request.
It is used for all Modbus type requests.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.