Technical FAQs

Ask a Question

Connexium Firewall Magic Number Incorrect

Title
Connexium Firewall Magic Number Incorrect message
 
Issue
Connexium Firewall Magic Number Incorrect message when downgrading firmware
 
Product Line
Connexium Industrial Firewall
 
Environment
Connexium
 
Cause
N/A
 
Resolution
 Regarding the "magic number incorrect" message: There are two hardware revisions of the Connexium Industrial Firewall in the field.
The newer hardware is based on EAGLE One family and the older configuration file is based on EAGLE 20 family and they are not compatible.
That means that the newer Connexium TCSEFEC product can not be downgrade with the older firmware files due to incompatibility.
Was this helpful?
What can we do to improve the information ?