Browse FAQs

Osisense XC - Cross-reference of the obsolete XCKP52112 and XCKP52113 limit switches

Published date: 06 June 2019

The obsolete XCKP52112 and XCKP52113 limit switches are special switches, based on the obsolete standard XCKP521 limit switch with cable entry Pg 11, and having a head orientation different from the standard switch. Attached picture of the XCKP52113 reference. Both references are replaced by the standard XCKP2521G11 limit switch, in which the head can be turned as you want.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.