Technical FAQs

Ask a Question

What is alternate and manual selection in Ecodial Advance Calculation?

Alternate solutions may be accessed only after a calculation has been validated.  If that is the case and the select another product command is launched, the selection window automatically opens the calculated products window. Then simply select the desired solution using the values proposed in the selection zone. The results zone is updated with the new solution. When OK is clicked, the solution is confirmed (locked), i.e. it will be used for future calculations.

A prior, validated calculation is not required to access solutions in the catalogue. If a calculation has not yet been validated, the selection window automatically opens the Entire catalogue window. If a calculation has been validated, Ecodial opens the Calculated products selection window. Select Entire catalogue to access the entire catalogue.
When a product is selected manually from the catalogue, it is "locked" for use in future calculations.
Was this helpful?
What can we do to improve the information ?