Browse FAQs

BMENOC03xx Status LEDS

Published date: 30 September 2019

Title
BMENOC03xx Status LEDS
 
Issue
BMENOC03xx Status LEDS
 
Product Line
BMENOC03xx M580
 
Environment
Unity Pro
 
Resolution
 The BMENOC03xx status LEDs are described below: There are also  two LEDs associated with each RJ-45 connector that indicate link status and activity.

RUN
green on - The module is configured.
off - There is no power to the module, or the module is not configured.
blinking - The module is in power-up test or in OS update.

ERR
red on - A detected error that is not an X Bus communication error.
off - There is no power to the module, no errors are detected, or the module is in OS update.
blinking - The module is not configured. An X Bus communication error is detected.

MS (module status)
off - There is no power to the module.
green on - The module is operating correctly.
blinking - The module is not configured.
red on - A major non-recoverable error (firmware error as an example) is detected.
blinking - A recoverable error is detected or the BMENOC03•1 has a duplicate IP address.

NS (network status)
off - There is no power to the module, or there is no link on all external ports including the Ethernet backplane port.
green on - At least one CIP connection for which the BMENOC03•1 module is the originator has been established.
blinking - The module has an IP address, but there is no CIP connection.
red on - The module has a duplicate IP address, or the module is in OS update.
blinking - At least one exclusive owner CIP connection (for which the BMENOC03•1 is the target) is timed out.
The LED blinks until the connection is reestablished or the module is reset

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.