Technical FAQs

Ask a Question

What is the heat dissipation value for the HMIG5U?

The caloric value of the product can be calculated with the following formula:

Calorific value=W[J/s]*[sec]=[J]

The power consumption values can be found in the user manual.


For example:According the OLH, the maximum power consumption (including the box module)  of the HMIDT642 is  56 W.

After 100 seconds, the calorific value is:

Calorific value=56 W[J/s]*100 [sec]= 5600[J] 
Was this helpful?
What can we do to improve the information ?