Technical FAQs

Ask a Question

Where we can find the ATV630 harmonic spectrum for drive ratings from 0.75KW to 315KW and the harmonic spectrum for 480VAC, 60HZ, 50KA drive supply?

Please find the updated Harmonic Spectrum in the excel files with ATVProcess THDi for drive rating from 0.75KW to 315KW. The harmonic spectrum for 480V/60Hz with 50kA drives also provided in the same attachment. These excel file is given as typical THDi for our ATV process drives
Was this helpful?
What can we do to improve the information ?