Browse FAQs

What is the M580 Syslog Server usage

Published date: 27 August 2019

Title
M580 Syslog Server usage
 
Issue
Operation of the M580 Syslog Server usage
 
Product Line
M580
 
Environment
Unity Pro
 
Resolution
 The M580 sends the syslog messages to the Syslog server setup in the Unity Project Setting. If the defined syslog server is not available over an extended period of time, it will not hinder the CPU.
There is a circular buffer of the events and the older events will be overwritten by the newer ones if the buffer is filled.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.