Technical FAQs

Ask a Question

How can I replace the fans on my Conext SW?

Issue:
Customer is looking for support on replacing the fans in their Conext SW

Product Line:
Conext SW series hybrid inverter/chargers
865-2524
865-4024
865-4048

Environment:
Any Conext SW with fan or overheating issues

Resolution:
The attached document includes information on replacing the fans. Order either part number 0J-0282 - Conext SW Fans Replacement Kit, or an equivalent fan using the specs below:

FAN 12VDC 370mA 85.2CFM 120x120x25mm 2200RPM 39.1dBA BALL-BEARING -10+75C

Cause:
Conext SW fan specs and replacement information not covered in standard documentation
Was this helpful?
What can we do to improve the information ?