Technical FAQs

Ask a Question

What would cause the ATV340 drive to trip on STO and not run?

Issue:
What would cause the ATV340 drive to trip on STO and not run?

Product Line:
ATV340 drive

Environment:
All 

Cause:
STO Inputs are open.

Resolution:
The STOA or STOB is not getting the 24vdc input.  Check the wiring at the top of the drive. 
 
Was this helpful?
What can we do to improve the information ?