Browse FAQs

Does the TM221C Logic Controller provide 24 Vdc supply to the inputs?

Published date: 16 August 2019

Issue:
What would cause the TM221C logic controllers inputs not to work?

Product line:
M221

Cause:
Clarification on wiring the inputs on the M221 and the input voltage.

Resolution:

Yes, the TM221C Logic Controller provides 24 Vdc supply to the inputs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.