Technical FAQs

Ask a Question

Can the Analog Inputs on the ATV18 be set up for reverse logic?

Issue:
Can the Analog Inputs on the ATV18 be set up for reverse logic?

Product Line:
Altivar 18

Environment:
All

Cause:
Need the drive to run at full speed when input is 0V and stop when input is 10V

Resolution:
The ATV18 does not have this functionality. 
Was this helpful?
What can we do to improve the information ?