Browse FAQs

What is a MSTR or MBP_MSTR operation 10 ?

Published date: 27 August 2019

Title
MSTR or MBP_MSTR operation 10
 
Issue
Purpose of the MSTR or MBP_MSTR operation 10
 
Product Line
Unity Pro
 
Environment
Unity Pro
 
Resolution
 The MSTR or MBP_MSTR operation 10 is a reset optional module operation causes a Quantum NOE Ethernet communications module or the Ethernet port on a 140CPU65150/60 CPU module to enter a cycle that resets its working environment. To program a MSTR or MBP_MSTR block to perform a reset option module operation, use function code 10

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.