Technical FAQs

Ask a Question

Can the BMXNOR0200H DNP3 Analog Input dead-band be adjusted from the PLC program ?

Title
BMXNOR0200H DNP3 Analog Input dead-band adjustment
 
Issue
BMXNOR0200H DNP3 Analog Input dead-band adjustment
 
Product Line
BMXNOR0200H M340 M580
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 Yes, you can adjust or change the BMXNOR0200H DNP3 Analog Input dead-band value from the PLC program if you add to the DNP3 Data Mapping a DNP3 Analog Input Deadband point that is assigned to the DNP3 Analog Input point number.
Was this helpful?
What can we do to improve the information ?