Technical FAQs

Ask a Question

Does Schneider Electric offer any type of gateway to interface between Modbus and control logic for out drives and soft starters?

Issue:
Does Schneider Electric offer any type of gateway to interface between Modbus and control logic for out drives and soft starters?

Product Line:
ATV61, ATV71 ATS48 etc

Environment:
All 

Cause:
Needs to interface between control net and modbus. 

Resolution:
Schneider Electric does not have a gateways to interface between control net and modubs  You will need to go thru Anybus.com  a 3rd party company to see if they still offer a Anybus X gateway adapter. 
Was this helpful?
What can we do to improve the information ?