Technical FAQs

Ask a Question

ConneXium Network Manager

Title
Connexium Network Manager license part numbers
 
Issue
Connexium Network Manager license part numbers
 
Product Line
Connexium Network Manager
 
Environment
Connexium Network Manager
 
Cause
N/A
 
Resolution
The latest version of the ConneXium Network Manager is version 2.0.
The latest Connexium Network Manager v2.0 does support the Windows Server 2012 platform.
Once you install this product you will have to purchase one of the licenses below to activate depending on the number of nodes required.

List of References part numbers for Full Licenses:

TCSEAZ03P002FM2    ConneXium Network Manager version 2.0 or higher 25 node
TCSEAZ03P010FM2    ConneXium Network Manager version 2.0 or higher 100 node
TCSEAZ03P050FM2    ConneXium Network Manager version 2.0 or higher 500 node
TCSEAZ03P100FM2    ConneXium Network Manager version 2.0 or higher 1000 node
TCSEAZ03P400FM2    ConneXium Network Manager version 2.0 or higher 4000 node

 

Was this helpful?
What can we do to improve the information ?