Technical FAQs

Ask a Question

Preventa XCS - Is the ​XCSRC*0M12 RFID contactless safety switch, single model, compatible with the XPSAF5130* safety relay

The ​XCSRC*0M12 RFID contactless safety switch, single model, is NOT compatible with the XPSAF5130* safety relay. It is compatible with the XPSAFL5130* safety module, able to monitor 2 OSSD's at the same potential. Please refer to the following table coming from the XCSRC user manual. Attached wiring diagram

Was this helpful?
What can we do to improve the information ?