Technical FAQs

Ask a Question

What would prevent process values from appearing in a Unity animation table?

One possible reason is that the section being examined is not being solved. Check to see if the section is disabled by doing the following.

 1: Go to the Project Browser
 2: Right click on the section name
 3: Select Properties
 4: Select "Condition"  

If there is a variable declared in the Condition field it will have the ability to allow the section to either solved or skipped..   
If a section is disabled and out of the normal logic solve there will be a red icon to the left of the section name when viewed in the Project Browser. 
Was this helpful?
What can we do to improve the information ?