Technical FAQs

Ask a Question

What would prevent process values from appearing in a Unity animation table?

One possible reason is that the section being examined is not being solved. Check to see if the section is disabled by doing the following.

 1: Go to the Project Browser
 2: Right click on the section name
 3: Select Properties
 4: Select "Condition"  
If there is a variable defined in the condition field it will have the ability to allow the section to solve, or skipped based upon the state of the variable.   
If a section is disabled and out of the normal logic solve there will be a red icon to the left of the section name . When the section is solving normally that icon will be green.
Was this helpful?
What can we do to improve the information ?