Technical FAQs

Ask a Question

Can SoMove 2.6.x be installed on a virtual machine?

Issue:
Can SoMove 2.6.x be installed on a virtual machine?

Product Line:
SoMove versions 2.6 and later

Environment:
Windows PC running VMware

Cause:
Customer needs to run SoMove on a VM

Resolution:
Yes, SoMove 2.6.x can be installed on a VM as long as the host OS is a supported version of Windows (7, 8.1,10), and the VM's OS is also a supported version of Windows. 
Please see the attached SoMove 2.6.4 Read Me file or the Read Me file for your current SoMove installation for further details. 



 
Was this helpful?
What can we do to improve the information ?