Browse FAQs

Does the M340 or M580 supports the addition of Static Routes to their Ethernet setup ?

Published date: 31 July 2019

Title
M340 or M580 and Static Routes
 
Issue
Can M340 or M580 add Static Routes
 
Product Line
M340 M580 BMENOC03x1 BMXNC0401 BMXNOE0100.
 
Environment
Unity Pro
 
Resolution
The M340 or M580 do not support the addition of Static Routes to their Ethernet setup. Static routes must be added to the external Gateway or Level 3 switch that is connected to the M340 and M580.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.