Technical FAQs

Ask a Question

What is exclusion in case of insulation monitoring devices that is taken care by XLI interface

The IMD injects a low frequency into the network. In a network with several incoming feeders, depending on the circuit breaker
position, there must be no more than one IMD injecting into the network. This injection exclusion is managed by the XLI300 interface.
Was this helpful?
What can we do to improve the information ?