Technical FAQs

Ask a Question

How can an Altivar drive run at a fixed speed without a external speed reference?

Issue:
How can an Altivar drive run at a fixed speed without a external speed reference?

Product Line:
Altivar drives

Environment:
All

Cause:
NA

Resolution:
One way this can be accomplished is by setting the low speed parameter in the drive to desired running speed, with no other speed reference the drive run at the low speed.
For example: If you program a drive with a low speed of 20Hz, then the drive will always run at a minimum of 20Hz any time a run command is given.
Was this helpful?
What can we do to improve the information ?