Browse FAQs

Unity DTM Compatibility Audit

Published date: 31 July 2019

Title
Unity DTM Audit Utility
 
Issue
Unity launches DTM Audit Utility to verify compatibility
 
Product Line
Unity Pro
 
Environment
Unity Pro
 
Resolution
 When opening a Unity program that was originally created from another version of Unity, The DTM Audit tool will display the DTM version used in the project.
To properly open that project the DTM on the PC must be equal to or greater than the DTM in the project.
You will not be able to open a Unity project if the DTM on the PC is lower than the DTM version in the project.
In the case where the PC version is lower, the user may need to install a Unity Hot fix or upgrade to a newer version of Unity in order to use the associated Unity project
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.