Technical FAQs

Ask a Question

Is there a way to implement an alternating scheme between two Altivar 212 variable speed drives without utilizing devices external to the drives?

Issue:
Is there a way to implement an alternating scheme between two Altivar 212 variable speed drives without utilizing devices external to the drives?

Product Line:
ATV212

Environment:
All

Cause:
NA

Resolution:
No. The ATV212 drive does not have a Pump Alternating function or scheme available. It needs to be done with external relays, timers or possibly a PLC. Another option is to select an ATV600 Series Drives.
Was this helpful?
What can we do to improve the information ?