Technical FAQs

Ask a Question

In Ecodial Advance Calculation, what is reactive power threshold parameter in power factor correction ?

This parameter determines the reactive power threshold above which power factor correction is required. If the reactive power consumed by the installation is less than this value, installation of power factor correction capacitors is not necessary even if the PF is less than the target PF.
The following two conditions must therefore be satisfied before Ecodial will carry out capacitor bank calculations:
PF < Target PF
Reactive power consumed > Threshold (50kvar) by default
Was this helpful?
What can we do to improve the information ?