Technical FAQs

Ask a Question

In Ecodial Advance Calcultaions, what are the configurations in electrical installations in which making cascading is impossible?

Below are the configurations in electrical installations making cascading is impossible in Ecodial Advance Calculations
1. The circuit breaker selected for cascading is supplied by two parallel circuits / sources.
2. The circuit breaker selected for cascading and the upstream circuit breaker are on opposite sides of a LV/LV transformer.
3. When a circuit breaker is supplied by circuit breakers operating under different operating modes, Ecodial does not attempt to find a cascading solution.
Was this helpful?
What can we do to improve the information ?