Technical FAQs

Ask a Question

What is the part number for a potentiometer to control Schneider Electric Altivar variable speed drives (VSDs) ?

 Issue:
What is the part number for a potentiometer to control Schneider Electric Altivar variable speed drives (VSDs) ?

Product Line:
Altivar ATV12, ATV212, ATV320, ATV630 and ATV930

Environment:
All

Cause:
Customer wanted to know what size of potentiometer should be used for his process drive ATV930?

Resolution:

 

The recommended specification for potentiometers compatible across our range of drives ATV12, ATV212, ATV320, ATV630 and ATV930 ( and the legacy ranges ATV15, ATV452, ATV16, ATV66, ATV18, ATV28, ATV58, ATV11, ATV31, ATV312, ATV21, ATV61 and ATV71) is 2.2k Ohms. It is possible to use a value between 2.2k Ohms to 10k Ohms in certain instances.

Schneider Electric can supply two potentiometers of the optimum value of 2.2k Ohms;
 

  • SZ1RV1202

 

Characteristics:


SZ1RV1202
2.2k Ohms - 3 Watts - IP65 - 9.5 mm cut-out
For use in dry environments on a wall-mounted or floor-standing enclosure.

See dimensions and mounting below.



 


 

 

 

Harmony style potentiometer mounting adapters
 

Schneider Electric offers IP66 potentiometer mounting adapters that compliment the Harmony diameter 22mm offer.
Two versions are available for potentiometers with shaft length 45 to 50 mm long and either 6mm or 6.35mm diameter shaft.

Part numbers;

ZB4BD912 (metal version) 6 mm diameter
ZB5AD912 (plastic version) 6 mm diameter

ZB4BD922 (metal version)  6.35 mm diameter
ZB5AD922 (plastic version)  6.35 mm diameter



Potentiometers to fit these adapters are not sold by Schneider Electric, they can easily be sourced at specialist distributors.

 


 
Was this helpful?
What can we do to improve the information ?