Browse FAQs

Is the GS2EEU3 Din rail mountable?

Published date: 25 February 2019

 Issue:
Customer ordered the GS2EEU3 understanding this was DIN rail mountable.  Now that they have in the field, there are two protrusions on the back preventing this from being installed on a standard DIN rail. 

Product line:
GS2EEU3

Environment:
n/a

Cause:
UL isolation requirements

Resolution:
For the UL certifications, Schneider needed to add isolation space between the poles.  To do this, extra spacers were added on the back of this switch to meet the UL requirements.  The GS2EEU3 is DIN Rail mountable, however the customer must use two separate sections of DIN rail to mount these.  In addition, the customer would be required to use screws in the mounting holes provided to secure the switch to the back of the panel. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.