Browse FAQs

9007C - What is the Y1901 form in the switch reference 9007C54DY1901 for example

Published date: 07 June 2019

Y1901 form = A single pole plug-in 9007C limit switch supplied with pre-wired mini 5 pin male connector Brad Harrison or equivalent. For use with female portable plug No. 41306, 41307, or 41308 (or equal). Not available with P10 or for hazardous locations

Male connector pin-out

Product picture


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.