Technical FAQs

Ask a Question

Why do I get an error P2057 when I try to add a Function Block to the project library?

After you export the function block to a library, you have to delete the function block instance in your app before you can add it back into your project library with the Library Manager.
Was this helpful?
What can we do to improve the information ?