Technical FAQs

Ask a Question

Are the M580, M340 and X80 modules rated with Class1 Div.2?

 Goals and Symptoms
 
are the M580, M340 and X80 modules complying with Class1 Div.2?
 
Facts and Changes
 
M580, M340, X80
 
 
Causes and Fixes
 
Marketing decided more than a year ago a strategy of certifying only M340 Harsh and Coated modules Class1 Div.2. That certificate was extended by CSA, who complies to CSA n°213, ISA 12.12.01 and FM3611.In addition, these ‘H’ and ‘C’ modules are also ATEX and IECEx zone 2, a little bit expensive but full hazloc.
 
Was this helpful?
What can we do to improve the information ?